2019-09-27 2:30 AM
Hi,
2019-09-27 3:02 AM
With a toolchains that supports this specific MCU. With special devices, you are usually bound to special tools.
Check the usual suspects (Keil, IAR, etc.). I don't know myself, never had a STM32H project.
I would be surprised if free tools like CubeIDE rush to support you here ...
2019-09-27 6:20 AM
Review the example/template projects provide in the CubeH7 HAL trees. Keil uses a single project with multi-target CM4 and CM7 build forks. Typically you build the CM4 side first and it gets bound with the CM7 side during the link operation.
2019-11-13 12:29 AM
Did you already check this document?
CubeIde is compiling now H745 Project. Im just waiting for a debugging manual like this.
2019-11-13 4:40 PM
Other STM32 didn't have as many problems with the ethernet drive as the H7. So the problem is the H7. The DTCM SRAM is the default system memory choosed by the CubeMX, and DTCM does not work with DMA for the H7. So you need change to AXI-SRAM and deal with cache coherency issues.
It would be nice if DTCM worked with DMA as it does in F7.
2019-11-13 6:09 PM
AC6 (openstm32) has been doing this for some months now.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.