cancel
Showing results for 
Search instead for 
Did you mean: 

How to power-supply the STM32H735-DK Discovery board when onboard st-linj-v3 is used? I found it in the documentation that it can consume over 700mA out of 5V

EDamm.1
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
TDK
Super User

Plenty of information about this in the user manual. Look at "6.2.2 Supplying the board from VIN: 7 V to 12 V/800 mA".

https://www.st.com/resource/en/user_manual/dm00682073-discovery-kit-with-stm32h735ig-mcu-stmicroelectronics.pdf

If you feel a post has answered your question, please click "Accept as Solution".
EDamm.1
Associate II

I have a 1000mA 5V Power-supply with micro-USB connector.

I want to plug this into the USB-OTG on the 735 an set the power-jumper to USB-OTG. The st-link v3 I connect to its connector on the 735.

Okay? ​

TDK
Super User

I'm fairly certain the user manual says you can only draw 500mA from the USB connector.

If you feel a post has answered your question, please click "Accept as Solution".
EDamm.1
Associate II

The STM32H735G-DK BOARD seamed to be debree now. It is unbeleaveable that the board will have to be powered by the arduino 5V female connector. How can it stand then on its 4 feed? I hope Digikey will take it back. ​

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.