2019-01-22 3:14 PM
I'm unable to successfully see my PWM signal on the Nucleo STM32F302R8 development board, connector 10, pin 37.
I have SB62 and SB59 connected with 0-ohm resistors. I don't understand why the same pin is on multiple pins. Absolute pin number 17 AND 18.
https://www.st.com/en/evaluation-tools/nucleo-f302r8.html
https://www.st.com/resource/en/schematic_pack/nucleo_64pins_sch.zip
Which solder bridges should I short?
2019-01-22 4:28 PM
Because the pins/functions are limited. PA2 is used for the VCP USART as well as the Arduino serial.
PA2 is CN10.35
PA3 is CN10.37
REMOVE SB13 (PA2) and SB14,SB58,SB53,SB62 (PA3)
MAKE SB63 (PA2) and SB59 (PA3)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.