2020-04-30 5:28 AM
Hi,
i'm using STM32H743 Nucleo Board, I'm new to it,
void (*Jump_To_application)(void);
volatile uint32_t BootAddr = 0x08020000;
void jump_To_sector()
{
/* Disable all interrupts */
__disable_irq();
/* Disable Systick timer */
SysTick->CTRL = 0;
SysTick->LOAD = 0;
SysTick->VAL = 0;
/* Set the clock to the default state */
HAL_RCC_DeInit();
SCB->VTOR = BootAddr;
Jump_To_application = (void (*)(void)) (*((uint32_t *) ((BootAddr + 4))));
__set_MSP(*(__IO uint32_t*)BootAddr);
Jump_To_application();
}
Please help me here to solve this.
Thanks in advance.
2020-04-30 7:09 AM
Did you change FLASH.ld file your application code?
2020-04-30 7:15 AM
yes, I changed Flash.ld file also.
this is the memory map
/* Specify the memory areas */
MEMORY
{
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
FLASH (rx) : ORIGIN = 0x08020000, LENGTH = 1024K
}
2020-04-30 7:16 AM
is there anything I need to change in FLASH.ld file? please let me know if any.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.