2021-02-22 7:32 AM
2021-02-22 7:35 AM
I'm using m24512 eeprom chip in stm32f303 i'm not able write and read the data from eeprom can you please suggest me
this my code
SLAVE addres is :0xA0
void i2c_master_write(uint8_t devAddr, uint32_t memAddr, uint8_t *i2c_WriteBuf, uint32_t length )
{
//TODO call HAL_i2c_Write function here
gM24512_TxBuf[0] = memAddr;
gM24512_TxBuf[1] = 0;
gM24512_TxBuf[2] = 0;
/*##- Start the transmission process #####################################*/
// do
// {
if (HAL_I2C_Master_Transmit_IT(&hi2c2, (uint16_t)devAddr, (uint8_t *)gM24512_TxBuf, sizeof(gM24512_TxBuf)) != HAL_OK)
{
/* Error_Handler() function is called when error occurs. */
//vcnl4200_Error_Handler();
}
/*##- Wait for the end of the transfer #################################*/
/* Before starting a new communication transfer, you need to check the current
state of the peripheral; if it’s busy you need to wait for the end of current
transfer before starting a new one.
For simplicity reasons, this example is just waiting till the end of the
transfer, but application may perform other tasks while transfer operation
is ongoing. */
while (HAL_I2C_GetState(&hi2c2) != HAL_I2C_STATE_READY)
{
}
please tell me anything i did miss
2021-02-22 8:14 AM
Hello
HAL_I2C_Mem_Read(...) and HAL_I2C_Mem_Write(...) functions are suitable for read and write to ser eeproms
uint8_t b[5];// define the buffer
HAL_I2C_Mem_Read(&hi2c, 0xA0, 0x0000, 2, b, sizeof(b), 100);// random read the first 5 bytes ( address=0)
parameters
hi2c is the I2C structure
0xA0 is the slave address (no need to shift 0x50<<1)
0x0000 is the adress of first byte (random addresses has 2 bytes)
2 is the length of the address (2 bytes long)
b is a pointer to buffer
sizeof(b) is the length of buffer
100 msec is the timeout for this operation if not succeed to return.. ( check the return value.)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.