2019-06-10 6:08 AM
i want to create a delay function using timer TIM1 or TIM2 , after completely reading the datasheet i cannot initialize delay does it requires any external input?
i have attached my sample code
#include "stm32f10x.h"
void delay();
int main()
{
/*Initialising Clock*/
RCC->CR = 0x00000103; //HSI Enable
RCC->CFGR = 0x051C0000; //HSI clock selected
RCC->CR = 0x01000103; //PLL enabled
RCC->AHBENR = 0x0001D057; //Clock Enable
RCC->APB2ENR = 0x00005E7D; //Clock Enable
RCC->APB1ENR = 0x3E7EC83F; //Clock Enable
RCC->CSR = 0x0C000001; //LSI Enabled
/* Initialising GPIO */
GPIOA->CRL = 0x11111111;
GPIOA->CRH = 0x11111111;
GPIOB->CRL = 0x11111111;
GPIOB->CRH = 0x11111111;
GPIOC->CRL = 0x11111111;
GPIOC->CRH = 0x11111111;
GPIOD->CRL = 0x11111111;
GPIOD->CRH = 0x11111111;
while (1)
{
GPIOA->ODR = 0x0000FFFF;
GPIOB->ODR = 0x0000FFFF;
GPIOC->ODR = 0x0000FFFF;
GPIOD->ODR = 0x0000FFFF;
delay();
GPIOA->ODR = 0x00000000;
GPIOB->ODR = 0x00000000;
GPIOC->ODR = 0x0000FFFF;
GPIOD->ODR = 0x0000FFFF;
delay();
}
}
void delay()
{
TIM2->CR1 = 0x0001; //Counter Enabled
TIM2->EGR = 0x0041; //Trigger generation & update generation enabled
TIM2->CNT = 0xFFFF; //Counter value set
TIM2->PSC = 0X0001; //Prescalar value set
TIM2->ARR = 0xFFFF; //Auto - Reload register set
}
2019-06-10 7:10 AM
No device, and TIMs, can run from HSI. HSE is not required, but needed if you want to run at 72 MHz.
You really can't jam values into the PLL like that.
If you choose to program the chip at the register level, you are responsible for reading and understanding the reference manual, and for debugging your own code.
Perhaps review the HAL or SPL code to provide a working/function context to compare your own implementation against.
2019-06-24 6:59 AM
HI
Thanks for the reply
I have tried to execute my code in different ways finally i come through the NVIC interrupt handlers, NVIC acts as the global interrupt hence only by activating the NVIC we are able to activate the interrupt anyway i want to enable my timer without interrupt and the timer doesn't gets initialized, why is initialization of NVIC necessary
2019-06-24 7:21 AM
Interrupts and NVIC are not required to use the TIM in a free running mode.
Your delay routine might actually have to do something, and wait for the time to elapse.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.