2021-02-26 1:23 AM
Hi,
I am using the STM32L151RCT6 in STM32cube IDE, i need to create MODBUS protocol communication between MCU and other board as slave..
Please suggest me any related link for implement this..
it will be helpful for me...
2021-04-06 3:13 AM
HI,
I am trying to pass float value from the MODBUS.
requirement is like i need to read adc data and after that i am converting it into voltage which is of float value .
That float value i need to map in MODBUS holding register and need to pass the float values from Modbus..
I am not getting how to manage the floats in the MODBUS register map , how to read float values from holding register and send???
Can you help me to fix this issue?
2021-04-12 1:01 AM
You don't have to worry about the mantissa and the exponent. Treat a float as a 4-byte integer by changing its type. In C language it is referred as type casting. An example is given below.
float x,y;
unsigned short int register1,register2;
register1= (unsigned short int)((unsigned int)x & 0xFFFF0000) >> 16; //(16 bit MSB)
register2= (unsigned short int)((unsigned int)x & 0x0000FFFF); //(16 bit LSB)
To recreate the float number, do the following:
y =(float) (((unsigned int)register1<<16) | (unsigned int)register2);
In my opinion this should work, but I haven't checked it out.
2021-04-20 11:01 AM
In (unsigned int)x casting a float to integer will get an integer part of float value. One can get a binary value by using address of a variable with ((uint16_t*)&x)[0] and ((uint16_t*)&x)[1] . But even better is a union type, which is dedicated for such purposes:
2024-01-26 7:56 PM
basically my sensor is 7 in 1 soil sensor to read the sensor data i am using the rs485 so at first i used to arduino it was worked so i need some support for interfacing the sensor for the stm32 b-l475e-iot01a ,where the sensor working on the modbus portocol
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.