2011-06-21 3:03 PM
I have three questions regarding clock configuration for the STM32F207 / STM32F217:
1. Is there any advantage to using any specific HSE frequency between 4MHz and 26MHz that is evenly divisible by 2, if the goal is to divide down to get the PLL input to 2MHz? (This is assuming I am using a quality low-jitter clock source to begin with.)
2. To get the lowest jitter 50MHz clock for RMII PHY use that can be produced by the STM32F2xx, wouldn't best practice be to feed the 2MHz into the I2SPLL?
3. Is there any document that shows what the expected jitter performance of the PLL is and how it is expected to vary as the input frequency changes from 1MHz to 2MHz? #stm32
2011-06-22 2:30 AM
There is some info in the F207/217 errata sheet about this issue. (PLL clock input is allowed to be higher than previously stated).
The solution I would prefer, if the PHY can do this (like the LAN8720A): Clock the PHY with the 25MHz crystal HSE output directly on MCO1 and let the PHY double the frequency and route this back to REF_CLK input. This way you avoid the PLL jitter completely. I must admit, I never tried this... try at your own risk...2011-06-22 9:50 AM
Or if there is a way of using an external 50 MHz source, which is stable, supplying that to the Ethernet interface, and dividing that by 2 to feed the STM32F2's clocks.
2011-06-22 4:47 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.