2008-09-13 10:53 AM
How to get into Standby Mode Simply
2011-05-17 3:44 AM
I believe I've boiled this down to a problem with my GCC toolchain.
See my more recent post where I show that it works fine using IAR4.42, but not GCC 4.2.0.2011-05-17 3:44 AM
I'm having trouble getting my stm32f101 into standby. Once there, I plan on waking up via a keypress on the wakeup pin, PA0.
While the example code uses the RTC and EXTI, I would like to do something simpler. I tried: /* Enable PWR clock and wakeup pin */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE); PWR_WakeUpPinCmd(ENABLE); myprintf (''entering standby mode after 2 seconds\r\n''); PWR_EnterSTANDBYMode(); When I run this, it appears to crash at this point, the oscillator stays running at full speed (HSI at 36mhz), I have a heartbeat LED driven off Timer1 IRQ and that keeps running. And a rising edge on PA0 doesn't do anything to get me out of this. What additional setup do I need to do to get into standby? My system only uses two interrupts (USART and Timer, both at priority 0 -- is this a problem?) ThanksWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.