2018-03-25 2:18 AM
With basic programming, now it can output some voice via 3.5mm one. But now don't know how to control the frequency of voice.
#voice2018-03-25 6:47 AM
Sorry which board specifically, link to it's home page because I'm assuming it is not the STM32L4R9I-DISCO
For tones you'd presumably make a pattern buffer with sine waves in it as a function of the CODEC/DAC sample rate and the lower frequency of the tone. The pattern buffer length being some integer multiple of sine waves so you can loop it and output a continuous signal.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.