2018-04-12 5:37 AM
Hai,
we are using a STM32F070RBT6 controller for development i need a clarification regarding I/O's
if we want use FT 5 V tolerant I/O we need add any external component or just enable has high.
Thanks
Rakshith
2018-04-12 6:26 AM
Whether a pin is 5V tolerant or not is due to the physical hardware of that pin - it is not configurable.
2018-04-12 6:39 AM
Hello
rakshith
,You may refer to table 'STM32F070xB/6 pin definitions' in the
to get the I/O structure.Khouloud.
2018-04-12 8:47 AM
It's a 5V I/o pin .we configured has high but we getting 1.6V..
Thanks
Rakshith
�Sent from TypeApp ​
2018-04-12 8:49 AM
See also section 6.3.14, 'I/O port characteristics' in the same document.
2018-04-12 8:56 AM
Your question, 'How to enable GPIO 5V tolerance' has been answered.
If your output is not driving to the expected level, that's a different question.
Suggest you mark this thread as answered, and start a new thread about your output drive problem.
But you will need to give a lot more detail for anyone to be able to help in that new thread:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.