2013-06-03 1:21 AM
Edit: Forumsoftware doesn´t work on mobile devices
2013-06-03 4:20 AM
Pretty much the same way you do for any other address range, you modify the linker and debugging scripts as required by the architecture and tools.
2013-06-03 1:23 PM
Hi
Sorry, I thought I wrote a short text in my priveous post, but obviously I submitted it uncorrectly. I'm working with ARM Keil and uVision IDE, there I set up the SRAM as the target location in the file options. Is that the correct method to do this? Another question: Then configuring the ST-Link, must I enter as Flash address the address of the SRAM or are some more settings required ? Regards JannisWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.