2024-02-05 3:56 AM
Hello Team,
I have implemented ADC_DMA (circular mode) Multiple channels in NUCLEO_H745 and in that added ethernet without RTOS when ethernet is implement ADC_DMA is not working it provide only one time data but i have configured for circular mode every 1HZ I need to get new data but after ethernet is implemented I am getting only I time data, So is there any memory mapping I need change any configuration in code?
PFA Below
Best Regards,
Gagan Gowda G R
Solved! Go to Solution.
2024-02-05 5:40 AM - edited 2024-02-05 5:40 AM
> SCB_InvalidateDCache_by_Addr((uint32_t *) &aADCxConvertedData_1[ADC_CONVERTED_DATA_BUFFER_SIZE], ADC_CONVERTED_DATA_BUFFER_SIZE);
This is problematic. Points to the end of the array, not the beginning, and has the incorrect size. May or may not be the problem.
SCB_InvalidateDCache_by_Addr(aADCxConvertedData_1, sizeof(aADCxConvertedData_1));
> hadc2.Init.ContinuousConvMode = DISABLE;
Possibly this should be enabled.
Disabling cache during the debugging process is an option.
2024-02-05 5:40 AM - edited 2024-02-05 5:40 AM
> SCB_InvalidateDCache_by_Addr((uint32_t *) &aADCxConvertedData_1[ADC_CONVERTED_DATA_BUFFER_SIZE], ADC_CONVERTED_DATA_BUFFER_SIZE);
This is problematic. Points to the end of the array, not the beginning, and has the incorrect size. May or may not be the problem.
SCB_InvalidateDCache_by_Addr(aADCxConvertedData_1, sizeof(aADCxConvertedData_1));
> hadc2.Init.ContinuousConvMode = DISABLE;
Possibly this should be enabled.
Disabling cache during the debugging process is an option.
2024-02-06 4:39 AM
Hello TDK,
Thanks a lot. The problem is resolved.
Best Regards,
Gagan Gowda, G R
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.