cancel
Showing results for 
Search instead for 
Did you mean: 

How to add arm_cfft_q31

leonardo
Associate III
Posted on May 08, 2017 at 00:27

I have a CubeMX generated project and need to made a FFT in Q31 format on a STM32F103RB nucleo board.

I have add this includes

#include <math.h>

#include 'arm_math.h'

#include 'arm_const_structs.h'

and add a defin ition for ARM_MATH_CM3

But as soon as I use

q15_t ADC_samples[2048];

arm_cfft_q15(&arm_cfft_sR_q31_len64, ADC_samples, 0, 1);

I get this error:

arm-none-eabi-gcc -mcpu=cortex-m3 -mthumb -mfloat-abi=soft '-D__weak=__attribute__((weak))' -DARM_MATH_CM3 '-D__packed=__attribute__((__packed__))' -DUSE_HAL_DRIVER -DSTM32F103xB -I'E:/Cartel_RGB/WS_F103/01_Cartel_F103/Inc' -I'E:/Cartel_RGB/Cartel_Lib' -I'E:/Cartel_RGB/WS_F103/01_Cartel_F103/Drivers/STM32F1xx_HAL_Driver/Inc' -I'E:/Cartel_RGB/WS_F103/01_Cartel_F103/Drivers/STM32F1xx_HAL_Driver/Inc/Legacy' -I'E:/Cartel_RGB/WS_F103/01_Cartel_F103/Drivers/CMSIS/Device/ST/STM32F1xx/Include' -I'E:/Cartel_RGB/WS_F103/01_Cartel_F103/Drivers/CMSIS/Include'  -Og -g3 -Wall -fmessage-length=0 -ffunction-sections -c -fmessage-length=0 -MMD -MP -MF'Src/main.d' -MT'Src/main.o' -o 'Src/main.o' '../Src/main.c'

../Src/main.c:77:14: error: expected declaration specifiers or '...' before '&' token

 arm_cfft_q15(&arm_cfft_sR_q31_len64, ADC_samples, 0, 1);

              ^

../Src/main.c:77:38: error: expected declaration specifiers or '...' before 'ADC_samples'

 arm_cfft_q15(&arm_cfft_sR_q31_len64, ADC_samples, 0, 1);

                                      ^

../Src/main.c:77:51: error: expected declaration specifiers or '...' before numeric constant

 arm_cfft_q15(&arm_cfft_sR_q31_len64, ADC_samples, 0, 1);

                                                   ^

../Src/main.c:77:54: error: expected declaration specifiers or '...' before numeric constant

 arm_cfft_q15(&arm_cfft_sR_q31_len64, ADC_samples, 0, 1);

                                                      ^

make: *** [Src/main.o] Error 1

Can some one explain how to add CMSIS-DSP lib to my project?

Thank

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Posted on January 16, 2018 at 11:36

Hi

Garberoglio.Leon

,

In the following doc

https://community.st.com/0D50X00009bMM6QSAW

, it is described how to add BSP in the generated CubeMX code... and especially how to add a folder in the CubeMX project.

I hope it will help you.

BR. Jeanne

View solution in original post

5 REPLIES 5
leonardo
Associate III
Posted on May 08, 2017 at 01:24

The problems seems to be around de CubeMX generated project.

In systemWorkbench I create a new empty project with HAL firmware, then add ARM_MATH_CM3 and add arm_cortexM3l_math library path and reference in Linker properties, finally I add this code:

#include 'stm32f1xx.h'

#include 'stm32f1xx_nucleo.h'

#include <math.h>

#include 'arm_math.h'

#include 'arm_const_structs.h'

int main(void)

{

    q31_t ADC_samples[2048];

    arm_cfft_q31(&arm_cfft_sR_q31_len64, ADC_samples, 0, 1);

    q31_t MAG_of_fft[1024];

    //arm_cmplx_mag_q15(ADC_samples, MAG_of_fft, 1024);

    for(;;);

}

and everithing compile ok.

So what could be happend with cube generated prject?

Posted on May 08, 2017 at 04:28

I have always had to manually copy the DSP library into my CubeMX projects.

Imen.D
ST Employee
Posted on May 08, 2017 at 16:57

Hi

Garberoglio.Leon

,

Which CubeMx/SW4STM32 version are you using ? You can share you .ioc file to check this issue.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on May 09, 2017 at 03:02

Is not a CubeMX problem.

I try with a new CubeMX generated project and simply add  arm_cortexM3l_math library and the include files and when I add a call to arm_cfft_q31 the program compile just fine.

So, the problem is when I add (link) a driver folder to the CubeMX generated project. I'm trying to identify the problem.

Whay os the best way to add a foolder with .c/.h files to a CubeMX project?

Thank

Posted on January 16, 2018 at 11:36

Hi

Garberoglio.Leon

,

In the following doc

https://community.st.com/0D50X00009bMM6QSAW

, it is described how to add BSP in the generated CubeMX code... and especially how to add a folder in the CubeMX project.

I hope it will help you.

BR. Jeanne

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.