2020-02-17 1:40 AM
Hi,
I am using the STM32G071KBU6N. It has the BOOT0 and SWCLK (PA14) on the same pin. Defined the pin as SWCLK in STM32CubeMX. So I assume that the SYS registers are set right in the software generation. However after the first download of the first firmware I can't reach the device any. Not via the UART1 nor via SWCLK (PA14) and SWDIO (PA13).
1. How can I reach the device again.
2. What should I change in the code to be able to reach the device next time.
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.