2022-07-06 2:40 AM
Hi,
I've used stm32flash on my processor with embedded Linux to program STM32U5 via USART. When I enter a command ./stm32flash /dev/ttymxc0 (usart interface connected to the STM32U5). I got a message "Failed to init device".
On the stm32flash site I found that stm32flash is missing support for STM32U575/U585 and that it is necessary to fill data about stm32u5 in dev_table.c file. In struct devices I need to fill: SRAM address range, FLASH address range, PPS (pages per sector), PSize (page size), Option byte address range, System memory address range and flags. I can't find any range for option byte address and how to fill flags field. Can you help me? How can I fill it? I tried to enter data without option byte address range and flags, but again message is "Failed to init device".
Is there any other program for serial programming stm32u5 from embedded linux? Has anyone managed to program stm32u5 via uart using stm32flash from embedded linux?
P. S. I read AN2606 and tried all combinations of bootloader activation pattern 12.
Thank you in advance,
Best regards,
Ana Savic
2022-08-10 5:32 PM
Hi Ana,
To be sure that the issue is not some missing files in Linux, did you tried the same with windows ?
I will check from my side also if someone already ran the use case in windows.
Best regards,
Younes
2022-08-10 5:40 PM
can you refer to ~STM32Cube_FW_U5_V1.0.0\Projects\B-U585I-IOT02A\Applications\OpenBootloader
project, may be it can help
Younes
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.