2015-05-12 4:28 AM
I am using external interrupts. STM32F407 is not handling interrupt at speed of greater than 2MHz.
/* Includes ------------------------------------------------------------------*/ #include ''stm32f4xx.h'' #include ''stm32f4xx_syscfg.h'' #include ''stm32f4xx_rcc.h'' #include ''stm32f4xx_gpio.h'' #include ''stm32f4xx_exti.h'' #include ''misc.h'' EXTI_InitTypeDef EXTI_InitStructure; void EXTILine0_Config(void); void LEDInit(void); void main(void) { LEDInit(); EXTILine0_Config(); EXTI_GenerateSWInterrupt(EXTI_Line0); while (1) { } } void LEDInit() { GPIO_InitTypeDef GPIO_InitStructure; RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE); /* Configure the GPIO_LED pin */ GPIO_InitStructure.GPIO_Pin = GPIO_Pin_15; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_Init(GPIOD, &GPIO_InitStructure); } void EXTILine0_Config(void) { GPIO_InitTypeDef GPIO_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; /* Enable GPIOA clock */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); /* Enable SYSCFG clock */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE); /* Configure PA0 pin as input floating */ GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; GPIO_Init(GPIOA, &GPIO_InitStructure); /* Connect EXTI Line0 to PA0 pin */ SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOA, EXTI_PinSource0); /* Configure EXTI Line0 */ EXTI_InitStructure.EXTI_Line = EXTI_Line0; EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure); /* Enable and set EXTI Line0 Interrupt to the lowest priority */ NVIC_InitStructure.NVIC_IRQChannel = EXTI0_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0x01; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x01; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); } void EXTI0_IRQHandler(void) { if (((EXTI->PR & EXTI_Line0) != (uint32_t)RESET) && ((EXTI->IMR & EXTI_Line0) != (uint32_t)RESET)) { GPIOD->ODR ^= 0x8000; EXTI->PR = 0x0001; } } Please help me!2015-05-12 5:27 AM
Yes, interrupting at 2 MHz is excessively high, you'd be entering the handler every few dozen machine cycles.
See if you can use a TIM peripheral to count or respond to input signals.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.