2012-09-18 4:53 PM
Hi every one
is anyone know about pulse capturing in stm32f4 ,how fast is it? and how accurate is it i wana measure 1mhz pulse with 0.2% error is stm32f4 able to do that?thank you2012-09-18 7:38 PM
No, I think you'd need a 500 MHz sample clock to do that, ie 2 ns granularity.
And you'd want a more accurate input clock. You could, I guess, integrate but that would require a series of pulses at the frequency rather than a singular pulse the question infers.2012-09-19 9:43 AM
thank you clive1
what frequency can i measure with 0.2% accuracy ?Is stm32f4 is suitable for measure frequency.I used of TIM_PWM_INPUT example but it's seems it doesn't accurate it's have big variation even in low frequency such as 20~60 khz.2012-09-19 9:44 AM
thank you clive1
what frequency can i measure with 0.2% accuracy ?Is stm32f4 is suitable for measure frequency.I used of TIM_PWM_INPUT example but it's seems it doesn't accurate it's have big variation even in low frequency such as 20~60 khz.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.