2017-11-26 5:15 PM
Good morning
I want to use uart in multiple ways as shown below.
I want to set prtinf tx and rx it with getchar.
How do I use multiple uarts with put char / get char?void UART_Init(void)
{huart1.Instance = USART1;
huart1.Init.BaudRate = 9600; huart1.Init.WordLength = UART_WORDLENGTH_8B; huart1.Init.StopBits = UART_STOPBITS_1; huart1.Init.Parity = UART_PARITY_NONE; huart1.Init.Mode = UART_MODE_TX_RX; huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart1.Init.OverSampling = UART_OVERSAMPLING_16; huart2.Instance = USART2; huart2.Init.BaudRate = 9600; huart2.Init.WordLength = UART_WORDLENGTH_8B; huart2.Init.StopBits = UART_STOPBITS_1; huart2.Init.Parity = UART_PARITY_NONE; huart2.Init.Mode = UART_MODE_TX_RX; huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart2.Init.OverSampling = UART_OVERSAMPLING_16; huart3.Instance = USART3; huart3.Init.BaudRate = 9600; huart3.Init.WordLength = UART_WORDLENGTH_8B; huart3.Init.StopBits = UART_STOPBITS_1; huart3.Init.Parity = UART_PARITY_NONE; huart3.Init.Mode = UART_MODE_TX_RX; huart3.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart3.Init.OverSampling = UART_OVERSAMPLING_16;huart6.Instance = USART6;
huart6.Init.BaudRate = 9600; huart6.Init.WordLength = UART_WORDLENGTH_8B; huart6.Init.StopBits = UART_STOPBITS_1; huart6.Init.Parity = UART_PARITY_NONE; huart6.Init.Mode = UART_MODE_TX_RX; huart6.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart6.Init.OverSampling = UART_OVERSAMPLING_16;}
void HAL_UART_MspInit(UART_HandleTypeDef* huart)
{GPIO_InitTypeDef GPIO_InitStruct;
if(huart->Instance==USART1) { /* USER CODE BEGIN USART1_MspInit 0 *//* USER CODE END USART1_MspInit 0 */
/* Peripheral clock enable */ __HAL_RCC_USART1_CLK_ENABLE(); /**USART1 GPIO Configuration PA9 ------> USART1_TX PA10 ------> USART1_RX */ GPIO_InitStruct.Pin = GPIO_PIN_9|GPIO_PIN_10; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF7_USART1; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);/* USART1 interrupt Init */
HAL_NVIC_SetPriority(USART1_IRQn, 0, 0); HAL_NVIC_EnableIRQ(USART1_IRQn); /* USER CODE BEGIN USART1_MspInit 1 *//* USER CODE END USART1_MspInit 1 */
} else if(huart->Instance==USART2) { /* USER CODE BEGIN USART2_MspInit 0 *//* USER CODE END USART2_MspInit 0 */
/* Peripheral clock enable */ __HAL_RCC_USART2_CLK_ENABLE(); /**USART2 GPIO Configuration PA2 ------> USART2_TX PA3 ------> USART2_RX */ GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_3; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF7_USART2; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);/* USART2 interrupt Init */
HAL_NVIC_SetPriority(USART2_IRQn, 0, 0); HAL_NVIC_EnableIRQ(USART2_IRQn); /* USER CODE BEGIN USART2_MspInit 1 *//* USER CODE END USART2_MspInit 1 */
} else if(huart->Instance==USART3) { /* USER CODE BEGIN USART3_MspInit 0 *//* USER CODE END USART3_MspInit 0 */
/* Peripheral clock enable */ __HAL_RCC_USART3_CLK_ENABLE(); /**USART3 GPIO Configuration PB10 ------> USART3_TX PB11 ------> USART3_RX */ GPIO_InitStruct.Pin = GPIO_PIN_10|GPIO_PIN_11; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF7_USART3; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);/* USART3 interrupt Init */
HAL_NVIC_SetPriority(USART3_IRQn, 0, 0); HAL_NVIC_EnableIRQ(USART3_IRQn); /* USER CODE BEGIN USART3_MspInit 1 *//* USER CODE END USART3_MspInit 1 */
} else if(huart->Instance==USART6) { /* USER CODE BEGIN USART6_MspInit 0 *//* USER CODE END USART6_MspInit 0 */
/* Peripheral clock enable */ __HAL_RCC_USART6_CLK_ENABLE(); /**USART6 GPIO Configuration PC6 ------> USART6_TX PC7 ------> USART6_RX */ GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF8_USART6; HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);/* USART6 interrupt Init */
HAL_NVIC_SetPriority(USART6_IRQn, 0, 0); HAL_NVIC_EnableIRQ(USART6_IRQn); /* USER CODE BEGIN USART6_MspInit 1 *//* USER CODE END USART6_MspInit 1 */
}}
2017-11-26 5:25 PM
Use sprintf() to a buffer, or use fprintf() and manage the FILE handle at the fputc() level in Keil
2017-11-26 6:42 PM
I do not understand well.
Could you show me the sample code?
2017-11-26 6:59 PM
/* Implementation of putchar (also used by printf function to output data) */
void SendChar(USART_TypeDef* USARTx, int ch) /* Write character to Serial Port */{ while(USART_GetFlagStatus(USARTx, USART_FLAG_TXE) == RESET); // Wait for EmptyUSART_SendData(USARTx, ch); // Send Char
}int fputc(int ch, FILE *f){ if (f == (FILE *)USART1) SendChar(USART1, ch); else if (f == (FILE *)USART2) SendChar(USART2, ch); else ITM_SendChar(ch);return(ch);
}fprintf((void *)USART1, 'Output USART1\n');
fprintf((void *)USART2, 'Output USART2\n');2017-11-26 7:07 PM
Thank you for your reply.
Excuse me, can I please sample rx?
2017-11-26 8:26 PM
Think about it a little, and consider how you can do similar things with fgetc()
Creativity is not about cut-n-pasting other peoples code.
2017-11-26 10:00 PM
Thank you for answer.
I've received a lot of help from your information.
Due to the short project deadline, I have asked many questions.
Have a nice day!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.