2018-07-02 12:02 AM
is it necessary to have dcmi interface on mcu to connect the camera?
2018-07-04 7:36 AM
Hello
hasithjp@gmail.com
,The
Nucleo-L476RG doesn&39t support Digital camera interface (DCMI).
So, you can emulate a parallel communication using GPIOs and DMA (see this application note
, which may help you for DCMI emulation).I recommend you to start using a board with DCMI interface, for that h
ave a look to this
Application note Digital camera interface (DCMI), which provides an explanation on the DCMI and related resources availability, a description of camera modules and their main components.
With Regards,
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.