2014-10-08 8:48 AM
Hi,
I'm using an stm32f401 mcu, mounted above Discovery platform, trying to understand how can I correctly use the standby low power mode; for this reason, I use the PA0 wake up to exit from this low power mode, but it doesn't work. The PA0, for my project, is setted as external interrupt, but when I use the standby mode, I configure it using the HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1) function that sets the EWUP bit in power control/status register, but when the mcu enter in standby mode and I push the button linked with PA0 pin, the mcu instead of restart code after the enter standby mode instruction, it resets. This is my code (only the code to enter/exit of standby mode):if
(f_EnterStdbyMode)
{
blink(3);
/* Set PDDS in power control register */
PWR->CR |= (uint32_t) 0x00000002;
/* Clear flaf wake up */
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);
while
((PWR->CSR & (uint32_t) 0x00000001)!=0);
//attesa che il WUF si azzeri (via HW)
/* Enable PA0 wake-up functionalities */
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN1);
HAL_PWR_EnterSTANDBYMode();
//<- qui il codice si ferma
HAL_GPIO_TogglePin(debugPin.port, debugPin.pin);
//<- qui il codice riprende la sua esecuzione
HAL_GPIO_TogglePin(debugPin.port, debugPin.pin);
/* Disable PA0 wake-up functionalities */
HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN1);
f_EnterStdbyMode =
false
;
blink(3);
} Please, can anyone tell me what's going on ?
Regards
2014-10-08 10:13 AM
STANDBY exits via a RESET, you catch it in main() or wherever when you check the reset cause.
2014-10-09 12:41 AM
Sorry but I'm a little bit confused; I read on reference manual:
''The microcontroller exits Standby mode when an external Reset (NRST pin), an IWDG Reset, a rising edge on WKUP pin, an RTC alarm, a tamper event, or a time stamp event is detected'' and in fact I use a wake up pin to exit from standby mode, but I don't know if it's possible to see it as a reset. Please could you explain me ?2014-10-09 1:00 AM
Hi
'Standby mode' basically powers down the processor (that is how it achieves the lowest power). So to wake up, you pretty much have to re-boot the whole thing. Yes, you can wake from standby with ''an IWDG Reset, a rising edge on WKUP pin, an RTC alarm, a tamper event, or a time stamp'' BUT you still have to go through the process of booting the processor again. So clive1 is correct - you have to catch the wake in your main loop or wherever when you check the reset cause.2014-10-09 1:11 AM
Could you give me an example of catching the reset cause ?
2014-10-09 1:33 AM
Hi
(Bear in mind this code is taken from my project for a STM32F405) // determine reason for reset (for reboots) uint32_t lastRstState = RCC->CSR; // code to detect a warm reboot (software reset) if ( RCC_CSR_SFTRSTF & lastRstState ) // watchdog reset else if( ( RCC_CSR_WDGRSTF | RCC_CSR_WWDGRSTF ) & lastRstState ) Please refer to the reference manual for the meaning of all of the bits in the RCC->CSR register2014-10-09 2:10 AM
Thanks a lot, I'll try immediatly this solution...only one question: why check the LPWRRSTF: Low-power reset flag of RCC control/status register, instead of SBF flag of power control/status register ? The last one remain unchanged after the exit of stand by mode
2014-10-09 2:48 AM
I tried both the flags but when the mcu resets, nothing happens, as I expected in my code:
int
main(
void
)
{
/* USER CODE BEGIN 1 */
uint32_t time;
char
str[15];
/* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* System interrupt init*/
/* Sets the priority grouping field */
HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_0);
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART2_UART_Init();
/* Check che l'avvio del sistema non sia stato causato da una precedente uscita
dalla modalità low-power standby */
if
(__HAL_PWR_GET_FLAG(PWR_FLAG_SB))
{
blink(3);
/* Clear flag */
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);
}
if
(__HAL_RCC_GET_FLAG(RCC_FLAG_LPWRRST))
{
blink(3);
HAL_Delay(800);
blink(3);
/* Clear flag */
__HAL_RCC_CLEAR_RESET_FLAGS();
}
2014-10-09 3:14 AM
''why check the LPWRRSTF: Low-power reset flag of RCC control/status register, instead of SBF flag of power control/status register ?''
No reason not to. It is up to you to work out the best way to determine if the processor has : Booted up from power on Re-booted due to reset (hardfault or software foreced) Wake from Standby. from the reset status bit and any other status registersWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.