2023-06-06 6:56 AM
Hi, I am using STM32G030K6T6 Microcontroller. I need a help for how can i Enable TDR Register and handle the interrupt handler. interrupt handler does not run and I need is Five Bytes data transmit in Uart_DMA. But registers does not wrk properly. I made a mistake anywhere please guide me. I include my code.
#include "main.h"
/* USER CODE BEGIN PV */
uint32_t data[5]={0x00,0x01,0x03,0x05,0x02}; uint16_t tim=0;
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
/* USER CODE BEGIN PFP */
void Tim3_Init(void)
{
RCC->APBENR1 |= RCC_APBENR1_TIM3EN; // TIM3 timer clock enable
TIM3->PSC = 2;
TIM3->ARR = 22999;
TIM3->CNT = 0;
TIM3->DIER |= TIM_DIER_UIE; //Update interrupt enable
NVIC_EnableIRQ(TIM3_IRQn); //Interrupt enable
TIM3->CR1 |=TIM_CR1_CEN; //COUNTER ENABLE
TIM3->EGR |= TIM_EGR_UG; //Update generation
}
void UART2_Init(void)
{
RCC->APBENR1 |= RCC_APBENR1_USART2EN; // USART2 clock enable
RCC->IOPENR |= RCC_IOPENR_GPIOAEN; // I/O port A clock enable
GPIOA->MODER &= ~(GPIO_MODER_MODE2); // clear 2th pin
GPIOA->MODER |= (GPIO_MODER_MODE2_1); // 10: Alternate function mode
GPIOA->MODER &= ~(GPIO_MODER_MODE3); // clear 3th pin
GPIOA->MODER |= (GPIO_MODER_MODE3_1); // 10: Alternate function mode
GPIOA->AFR[0];
GPIOA->OTYPER |= (0<<2); // output_pushpull
USART2->CR1 |= USART_CR1_TE;
USART2->CR3 |= USART_CR3_DMAT; // DMA TX_ENABLE FOR USART2
USART2->BRR |= 0X1D4B; // BAUDRATE
USART2->CR1 |= USART_CR1_UE; //USART_ENABLE
}
void DMA_Init(void)
{
RCC->AHBENR |= RCC_AHBENR_DMA1EN; //DMA1_MUX_CLK_Enable
// SYSCFG->IT_LINE_SR = SYSCFG_ITLINE9_SR_DMA1_CH1;
DMA1_Channel1->CCR |= DMA_CCR_MINC | DMA_CCR_TCIE | DMA_CCR_DIR | DMA_CCR_CIRC | DMA_CCR_TEIE | DMA_CCR_HTIE ; // MEMORY_INC, TX_COMP_INT, DATA_TX_DIR, CIRCULAR_MODE
DMA1_Channel1->CPAR = (uint32_t)&USART2->TDR;
DMA1_Channel1->CNDTR=5;
DMA1_Channel1->CCR|= DMA_CCR_EN;
NVIC_EnableIRQ(DMA1_Channel1_IRQn);
}
void tx(char tx_data)
{
USART1->TDR= tx_data;
while(!(USART2->ISR & (1<<6)));
}
void DMA_transmit(char data, uint8_t size)
{
DMA1->IFCR |= DMA_IFCR_CTCIF1; // channel tx complete clear
DMA1_Channel1->CMAR =(uint32_t)data;
}
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
/* USER CODE BEGIN 2 */
Tim3_Init();
UART2_Init();DMA_Init();
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
void DMA1_Channel1_IRQHandler(void)
{
while((DMA1->ISR & DMA_ISR_TCIF1)==0);
DMA1_Channel1->CMAR =(uint32_t)data;
DMA1->IFCR =DMA_IFCR_CTCIF1; // channel tx complete clear
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV1;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV1;
RCC_OscInitStruct.PLL.PLLN = 8;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief GPIO Initialization Function
* @param None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/*Configure GPIO pin : PC15 */
GPIO_InitStruct.Pin = GPIO_PIN_15;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF1_OSC;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
}
/* USER CODE BEGIN 4 */
void TIM3_IRQHandler(void)
{
TIM3->SR &= ~TIM_SR_UIF;
tim++;
}
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
__disable_irq();
while (1)
{
}
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.