2022-06-28 12:31 AM
2022-06-28 9:48 AM
Hi @felix ,
I confirmed the issue, there is mistake in these datasheets: DS12712 and DS12997.
The pin description list is the correct one:
For Pin PA10, the alternate function is I2C2_SMBA.
For Pin PA8, the alternate function is I2C2_SDA. I reported this issue internally.
Internal ticket number: 131036 (This is an internal tracking number and is not accessible or usable by customers).
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-06-28 7:36 AM
I think you are right ... congratulations for this ... I never saw an error in these lists before - usually I think (hope :) ) they are checked very very carefully..
In the Pin description list PA8 shows "I2C2_SDA" and PA 10 shows "I2C2_SMBA" (same datasheet, chapter 4.10), but in the Alternate function list (chapter 4.11) for I2C2 these two functions at PA8/PA10 are just mixed up!
2022-06-28 9:48 AM
Hi @felix ,
I confirmed the issue, there is mistake in these datasheets: DS12712 and DS12997.
The pin description list is the correct one:
For Pin PA10, the alternate function is I2C2_SMBA.
For Pin PA8, the alternate function is I2C2_SDA. I reported this issue internally.
Internal ticket number: 131036 (This is an internal tracking number and is not accessible or usable by customers).
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.