2023-05-23 10:40 PM
2023-05-24 12:15 AM
Do you mean a MEMS oscillator with active full-swing output?
If yes, that should work as with any other oscillator.
Anyway, check the STM's datasheet for maximum HSE input frequency.
2023-05-24 12:59 AM
Accorcing to datasheet, HSE clock value is between 4-48MHz.
Clock referance part number is given at AN2867 however HSE clokc is not mentioned.
Therefore ı asked this question.
Can ı place active oscillator (MEMS, part number ASFLMB-48.000MHZ-LR-T ) instead of 48MHZ crystal (part number ABM8G-48.000MHZ-18-D2Y-T)?
2023-05-24 1:35 AM
That should work, it looks like the ASFLMB-48.000MHZ-LR-T exactly behaves like an oscillator.
Just curious: why do you want to use a MEMS oscillator? It will definitely draw a few more mA.
Although the MEMS oscillators have become quite good over the years, I'm currently using a MEMS VCO.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.