2022-09-18 12:57 AM
2022-09-18 5:55 AM
ok. look at mouser : STM32 + LQFP 64 or 100 - > 800 types, choose yourself !
... or ask a friend for help.
2022-09-18 9:12 AM
The entire STM32 range have UARTs capable of beyond 230400 baud
Likely will need a 64 or 100-pin device to get 44 GPIO, there are also larger parts if you need to bank groups of GPIO pins, or simplify routing.
Low Cost means what? Availability issues have some parts at x5 or x10 over retail
Most everything is likely to have a 40-50 week lead time, perhaps narrow to what you can source and afford?
2022-09-18 10:44 AM
Try STM33G0 family.
2022-09-18 8:20 PM
2022-09-18 8:46 PM
Probably should have lead with that, not the right forum.
Perhaps have your engineer(s) evaluate what it is you need, and what meets those goals.
2022-09-18 11:29 PM
Hi Team,
I need an 8bit controller (Through hole) with a baud rate of 230400 and require a minimum of 30 GPIOS. Kindly suggest me a part suitable for this.
Best Regards,
Aswin
**Edited by moderation - Please do not share personal info in a public post**
2022-09-19 5:06 PM
You are asking for an 8-bit microcontroller in a STM32 (32-bit) section. Also no memory sizes and package types mentioned. And what's the problem with opening the STM8 web page and at least setting up some filters?
https://www.st.com/en/microcontrollers-microprocessors/stm8-8-bit-mcus.html#products
2022-09-19 5:34 PM
Do people make a lot of MCU in 40 or 48-pin DIP these days?
Surely a lot of these wish items would seem to significantly limit your choices.
Needs 5V ?
Why would it matter is the MCU is 8, 16 or 32-bit ?
Perhaps someone can fab you a board in the form-factor of an old DIP you can use?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.