2019-06-27 12:13 AM
2019-06-27 12:45 AM
Being more descriptive with your issue, already at the headline, would help a lot.
The STM32 discovery boards use to have ST-Link debug adapters, not OpenOCD.
Or do you have replaced the ST-Link firmware on your board ?
2019-06-27 1:15 AM
Looks like you are using wrong setup files for openOCD. Which debug interface are you using?
At least SWD should work fine with OpenOCD - I've been using the Eclipse-OpenOCD-ST-link-mini for quite a while.
There could also be ST-link USB-driver missing.
What's your board? Are you using ST-link-v2? Or maybe an on-board debug HW?
2019-06-27 2:57 AM
No..I did not replaced the st-link
2019-06-27 2:58 AM
I am also using the same. Eclipse-OpenOCD
2019-06-27 3:42 AM
Hello,
Thanks for the reply .
my settings are
board : STM32F407VGTX DISCOVERY BOARD (old)
I downloaded the latest AC6 system workbench from openstm32.org
i also installed stlink drivers from here https://www.st.com/en/development-tools/stsw-link009.html
and interestingly it works on other PC but having issue on mine.
I dont understand what is missing in my PC ?
2019-06-27 4:05 AM
@jennifer_dsilva you created this post 3 times, so I deleted the other two posts. Please only post a question once; otherwise it is a mess if people start responding in several places, thanks!
Also as mentioned, when you post a question, please describe:
2019-06-27 5:39 AM
Can't you configure your project to use the ST-Link debugger instead ?
Would be the easiest way.
2019-06-27 5:43 AM
> ... you created this post 3 times, so I deleted the other two posts. Please only post a question once; otherwise it is a mess if people start responding in several places, thanks!
I use to blame the awkward and un-intuitive forum software.
Not that it hadn't been mentioned, but there are nice and stable forum platforms available. (Just check some competitiors ... :o )
Why has ST to come up with something extraordinary each time ?
2019-06-30 1:59 AM
Maybe your OpenOCD configuration file is wrong?
In debugger tab (don't remember by heart) there should be something like "-f boards/stm32f4discovery.cfg"
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.