2021-08-11 6:16 PM
2021-08-11 8:27 PM
Is your code actually running?
BOOT0 Pulled Low?
Stuck in some loop waiting for clocks and PLLs to start?
What happens if you just continue with the HSI or MSI clock source the MCU started with?
2021-08-12 1:30 AM
//This is my code
// could you please check it
#include "stm32f4xx.h"
#define PLLM 25
#define PLLN 320
#define PLLP 1//divide 4
int clock_80MHz_Ex_pll();
int pinMode();
void InitTIM2();
void Delay_us();
void Delay_ms(int x);
int clock_80MHz_Ex_pll()
{
RCC->CR|=RCC_CR_HSEON;//External Crystal Oscillator
while(!(RCC->CR & RCC_CR_HSERDY));// External Crystal oscillator status flag checking
RCC->APB1ENR|=RCC_APB1ENR_PWREN;// power Enable
PWR->CR|=PWR_CR_VOS;// voltage scaling
FLASH->ACR|=(FLASH_ACR_DCEN|FLASH_ACR_ICEN|FLASH_ACR_PRFTEN|FLASH_ACR_LATENCY_2WS);
RCC->CFGR|=(RCC_CFGR_PPRE2_DIV1|RCC_CFGR_PPRE1_DIV2|RCC_CFGR_HPRE_DIV1);
RCC->PLLCFGR|=(PLLM<<0|PLLN<<6|PLLP<<16|1<<22);
RCC->CR|=RCC_CR_PLLON;
while(!(RCC->CR & RCC_CR_PLLRDY));
RCC->CFGR|=RCC_CFGR_SW_PLL;
while(!(RCC->CFGR & RCC_CFGR_SWS_PLL));
return 1;
}
int pinMode()
{
RCC->AHB1ENR|=RCC_AHB1ENR_GPIOCEN;
GPIOC->MODER|=0x55555555;
GPIOC->OTYPER=0;
GPIOC->OSPEEDR=0;
return 0;
}
void InitTIM2()
{
RCC->APB1ENR|=(1<<0);//Enable timer 2
TIM2->PSC =79;
TIM2->ARR=0xFFFF;
TIM2->CR1 |=(1<<0);
}
void Delay_us()
{
TIM2->CNT=0;
while(TIM2->CNT < 1000);
}
void Delay_ms(int x)
{
for(int i=0;i<x;i++){
Delay_us();}
}
int main()
{
clock_80MHz_Ex_pll();
pinMode();
InitTIM2();
while(1){
GPIOC->ODR=(1<<13);
Delay_ms(1000);
GPIOC->ODR=~(1<<13);
Delay_ms(1000);
}
return 0;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.