2020-08-08 5:49 AM
I need to generate:
Do you think that core of this MCU is able fulfill these tasks? Is necessary to choose another one or not.
Thank you very much.
Best Regards,
Miro
2020-08-08 6:41 AM
So, you want 300MHz timers, and 7 individual 2MSps ADCs - yet you are concerned about the processor core?
JW
2020-08-08 7:54 AM
Only the H7 is going to be able to have a 300MHz timer, which is going to be required to do 3MHz at 1% duty cycle. And even then, only with the HRTIM peripheral.
If you are more flexible on the frequency, or the PWM resolution, you will have more options.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.