2016-12-12 7:35 PM
Hi,
I'm using IAR to create a hex file which size is 233KB.
However, when I look into the .map file, it told below:
183 710 bytes of readonly code memory
4 265 bytes of readonly data memory
62 327 bytes of readwrite data memory.
The ROM size is 183710+4265=187975.
This is not the same with hex file size.
Which one is correct?
Thanks.
2016-12-12 7:59 PM
My guess would be all of them are correct.
Your .hex file is a representation of your program's machine code binaries. Each byte is represented by two displayable ASCII values with a value of 0-F. Then the file has the addresses of where the values should go, byte counts, record types, checksums, and a whole whack of colons.
Take a look at the wikipedia entry for Intel Hex Format and all will be revealed.
https://en.wikipedia.org/wiki/Intel_HEX
Andrei from The Great White North
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.