2012-04-11 9:48 AM
Hi everyone,
I'm very new to STM32 Discovery and I want to do some project with it. I need to capture PCM signal(voice) from GTM382 modem before it reaches CODEC. I know there is PINS:MCLK - 2MHzPCMSYNC - 8 kHzPCMI - PCM input, which is devided into 8 byte slots.So I need to overtake it, I need to make STM32 Discovery clock work simultanously with GTM382 modems' (2MHz) and PCMSYNC will show me when is begining of new slot of 8 bytes(flag), so I need to take the stream correctly and send it to PC (make a .wav file). Please help. Any suggestions? #!surprised #gtm382 #adc-stm32-discovery2012-04-11 10:01 AM
As an SPI or I2S slave perhaps?
2012-04-11 10:10 AM
SPI.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.