cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, We have implemented MDIO(Management Data Input/Output) protocol by bit banging in the STM32 Nucleo-L series board and the corresponding frequency of MDIO is 2.8MHz as of now.

sa.2
Associate

0693W00000Y7MKmQAN.pngMy requirement is to increase this frequency since the MCU (Arm® Cortex®-M33) operates at 110MHz. Kindly, share your inputs ?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
MM..1
Chief III

L??? try show code ...

KnarfB
Super User

such high frequencies are typically generated by hardware peripherals, not by software (bit banging). Search for timer dma pwm or timer dma gpio

hth

KnarfB

Lina_DABASINSKAITE
Community manager

Hi @sa.2​ ,

Thank you for being ST Community Member!

I noticed you raised the same questions twice. As our goal is to not have duplicated discussion, we are closing this thread and direct everyone to discuss the questions it further here.

Lina from ST Community Team


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.