2021-02-26 12:11 AM
2021-02-26 12:19 AM
Most likely no, but you should check yourself in the Datasheet.
JW
2021-02-26 2:13 AM
Hello @lazzo.1 ,
As said by Jan, the datasheet is your reference to compare the peripherals and pinout.
For the difference between the peripherals, you can also use the ST-MCU-FINDER Tool that provides a part number shortlist based on the user selection of peripherals and MCU characteristics. So, you can compare the characteristics of both MCU.
Imen
2021-02-26 3:25 AM
If the MCUID of the parts is the same, they are the same die.
2021-02-26 4:20 AM
They still could be bonded out differently, though...
JW
2021-02-26 4:57 AM
But for the same package and the same family that is very unlikely...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.