2019-10-21 12:07 PM
2019-10-21 12:14 PM
The easiest is to use UART, and then some UART-to-USB converter.
JW
2019-10-21 12:25 PM
Thanks for the help, waclawak.jan!
I've got an USB TTL converter, but I have one doubt:
I will program by STMCube using a ST-Link, and after change ST-link to USB-TTL conveter do get data?
2019-10-21 8:15 PM
ST-Link and the UART to USB would generally be hooked up to different pins. They could both be connected at the same time.
Newer boards with built in ST-Link include a VCP which does the UART to USB conversion as well.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.