2014-09-17 12:55 AM
Hi All,
Has anyone ported Helix MP3floating
point to F4 to utilise the FPU?If not, has anyone have a comment on the performance difference between the Helix fixed point and the floating point versions using the FPU in F4.FYI: I am not converting one audio stream, but multiple and as fast as possible. I already know F4 is more than capable for at least one audio stream using fixed pt.I just want to know if spending time converting MP3 fxt pt to floating pt for F4 is going to be worthwhile.Thx Jason2014-09-17 2:13 AM
I can't give you a specific answer, but note, that the floating point support in STM32F4xx is only for 32-bit (aka single-precision, binary32, ''float'' in C) floating-point variables rather than the more common 64-bit (double-precision, binary64, ''double'' in C) ones. Thus, ''double'' arithmetics is performed in software with no hardware support.
This usually comes as a surprise to many who come from the PC/''big embedded'' world. JWWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.