2011-03-28 12:08 AM
Heap size
2011-05-17 5:29 AM
This is a standard 'C' term; it has nothing specifically to do with the STM32 - or even with embedded development!
The Heap is the term used for the memory ''pool'' available for dynamic memory allocation by the standard 'C' library functions such as malloc''how does heap size effect my project? how to set it ? usage of it ?''
That depends on the particular tools you are using''Could you give a quik veiw please ?''
You will need to study the manuals for the particular tools that you are using. Note that dynamic memory allocation is often best avoided on embedded systems...
2011-05-17 5:29 AM
Thank you Neil
I am using uv4 (keil ) ; I could dont find info about heap in the manual , could you give a link or a short info please ? what is the effect of small heap and large heap on a project ?2011-05-17 5:29 AM
http://www.keil.com/forum/18655/
2011-05-17 5:29 AM
what is the effect of small heap and large heap on a project ?
The size of the heap constrains the total capacity of malloc()'s you can have outstanding. If you fragment the heap, your total/linear capacity will be diminished, as it will if you leak resources (fail to free). With GNU/GCC the heap basically takes all the unallocated RAM between your statics, and your stack.http://www.lmgtfy.com/?q=embedded+software+heaps
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.