2016-11-29 4:23 AM
if i call the assembly instruction ''sub sp, sp, 0xF8'' alias ''BE B0'' (instruction code), the code is executed as a ''nop''. Checked with F103 and L471.
Does anyone know about that or can confirm this? Is the assembly ''sub sp, sp, 0xF8'' forbidden? ''sub sp, sp, 0xF4'' or ''sub sp, sp, 0xFC'' are working correctly! Is there a way to forbid the compiler to use this specific command?2016-11-29 5:18 AM
Seems to be a debugger fault (why ever?).
2016-12-05 6:30 AM
Dear damh,
Could you share your debugger screenshot ? and see what is really executed by the core in the Cortex-M3/M4 registers .
cheers,
2016-12-05 11:17 AM
are you running in user mode rather than supervisor mode? The SP register may be protected as a special register unless you are running with the right privileges. The chip by default comes up in supervisor mode, but if anything in your startup code, or later, changes this you could be dealing with a violation of the rules of the chip during operation that would not show up in the assembler since the latter does not know the context in which you will run the code.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.