2015-01-04 12:22 AM
Dear friends.
My platform is STM32F429Discovery.
I encountered whit Hard Fault error. I used the code of Joseph Yiu to track the place where error occurs. It is in the portasm_cm4.s (FreeRTOS).
ldr r0, [r1]
r1=0x03FF6BF7, and this part of memory is reserved, so the HardFault is generated.
What is my next step?
Here is the full function:
xPortPendSVHandler:
mrs r0, psp
/* Get the location of the current TCB. */
ldr r3, =pxCurrentTCB
ldr r2, [r3]
/* Is the task using the FPU context? If so, push high vfp registers. */
tst r14, #0x10
it eq
vstmdbeq r0!, {s16-s31}
/* Save the core registers. */
stmdb r0!, {r4-r11, r14}
/* Save the new top of stack into the first member of the TCB. */
str r0, [r2]
stmdb sp!, {r3, r14}
mov r0, #configMAX_SYSCALL_INTERRUPT_PRIORITY
msr basepri, r0
bl vTaskSwitchContext
mov r0, #0
msr basepri, r0
ldmia sp!, {r3, r14}
/* The first item in pxCurrentTCB is the task top of stack. */
ldr r1, [r3]
ldr r0, [r1]
/* Pop the core registers. */
ldmia r0!, {r4-r11, r14}
/* Is the task using the FPU context? If so, pop the high vfp registers
too. */
tst r14, #0x10
it eq
vldmiaeq r0!, {s16-s31}
msr psp, r0
bx r14
2015-01-04 5:46 AM
What is my next step?
Determine why the process's stack context is getting corrupted.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.