2018-08-22 6:46 AM
Can someone translate this, and dumb it down for me a little please?
I am just trying to get my very basic, very simple SPI slave to receive a bunch of bytes from a PC application using interrupts.
After receiving the first byte the code goes into the infinite loop in the HardFault_Handler() function.
If I pause the program before any bytes have come, then the program acts normally. However, if I pause execution after 6 bytes of data, then I find myself inside that infinite loop. And I can see that only a single byte has been read.
But then why is PC zero?
I did not touch any HAL libraries. And I will paste you my code at the end.
I am using:
. STM32L4R7VIT
. IAR for ARM 8.30.1.17148
Thank you very much.
Fault Exception Viewer:
----------------------------------
The processor has escalated a configurable-priority exception to HardFault.
An instruction executed with an invalid EPSR.T or EPSR.IT field (CFSR.INVSTATE).
Exception occured at PC = 0x0, LR = 0x80066b7
See the call stack for more information.
Call Stack:
---------------
HardFault_Handler
<Exception frame>
[PC = 0x00000000]
My Code:
-------------
extern SPI_HandleTypeDef hspi1;
void init_spi(void)
{
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_SLAVE;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_HIGH;
hspi1.Init.CLKPhase = SPI_PHASE_2EDGE;
hspi1.Init.NSS = SPI_NSS_HARD_INPUT;
// hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_128;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 7;
hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi1.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
hspi1.RxISR = spi1_int_handler;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
SET_BIT((hspi1.Instance->CR2), SPI_RXFIFO_THRESHOLD_QF);
__HAL_SPI_ENABLE(&hspi1);
__HAL_SPI_ENABLE_IT (&hspi1, SPI_IT_RXNE);
__HAL_SPI_DISABLE_IT(&hspi1, SPI_IT_TXE);
__HAL_SPI_ENABLE_IT (&hspi1, SPI_IT_ERR);
// Enable the SPI global interrupt.
HAL_NVIC_EnableIRQ(SPI1_IRQn);
}
void spi1_int_handler(SPI_HandleTypeDef *hspi)
{
HAL_SPI_Receive(hspi, &rx_byte, 1, 1000);
debug_buf[debug_buf_ix++] = rx_byte;
}
2018-08-22 8:28 AM
Suggests you don't have a SPI1_IRQHandler() function set up properly.
Likely not the code you're actually showing..
but would scope the access to debug_buf[] so it doesn't go off the reservation.
2018-08-22 8:45 AM
Thanks very much for your attention.
I already made this correction to my original post, and in the code:
__HAL_SPI_ENABLE_IT (&hspi1, SPI_IT_RXNE);
...
However, I changed the code to read data in a while loop, which for my application makes more sense than interrupts and which alleviates the problem. Besides, I wasn't able to get the interrupts working anyway. I wish there was a code example on the ST site that showed basic SPI operation.
Later on I will experiment with the code again and let you know if the problem shows up again.
Thanks a lot,
Za
2018-08-22 4:06 PM
Yes, I agree with @Community member this line looks suspect..
debug_buf[debug_buf_ix++] = rx_byte;
where do you check that debug_buf_ix is not out of range ?
normally:
debug_buf_ix++;
if ( debug_buf_ix > 1000) debug_buf_ix =0; //circular buffer.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.