2011-03-23 2:10 AM
Hard Fault problem
2011-05-17 5:29 AM
08002ace: str r2, [r3, #0] << Could it be faulting here. What is in R3?
2011-05-17 5:29 AM
2011-05-17 5:29 AM
Yes, the problem was that!
There was an uninitialized pointer :( And it wasn't signaled by the IDE!! :( :( I did a lot of noise for a stupid problem... Sorry! Thaks Clive1 for the illuminating hint! :) I.2011-05-17 5:29 AM
No problem, you'll catch it the next time.
NULL or invalid pointers are a classic cause of Hard Faults, and the address you were pointing to looked just fine. So I looked at the next most likely reason. Was Atollic pointing you at this address, or do you have some fault handler code, like Joseph Yiu's example?2011-05-17 5:29 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.