2015-11-17 12:13 PM
Greetings,
So I decided to play with the RTCex library, specifically the much abbreviated new timer_IT function. My system is designed to shutdown after every code iteration and be awakened via the alarm(wakeup timer).The issue is, the timer only works up to 30seconds. I can input any counter up to that point and the system wakes near the specified time. Not sure why, other than maybe I'm catching a edge at that point somehow. Thoughts? I've tried changing the RTC config parameters as well (WAKEUP, PUSHPULL, etc), to no avail.Here is my code so far:&sharpdefine ALARM_TIMER ox1E046 //60s (considering 16MHz clock, using LSI) __HAL_RCC_PWR_CLK_ENABLE(); HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);__HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(&hrtc, RTC_FLAG_WUTF); /*♯♯ Setting the Wake up time ♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯♯*/HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, ALARM_TIMER,RTC_WAKEUPCLOCK_RTCCLK_DIV16); /* Request to enter STANDBY mode */HAL_Delay(3000);HAL_PWR_EnterSTANDBYMode(); //***ENTER STANDBY***//Configuration is thus (as recommended by another RTCex thread and CubeMX):void MX_RTC_Init(void){ /**Initialize RTC */ hrtc.Instance = RTC; hrtc.Init.HourFormat = RTC_HOURFORMAT_24; hrtc.Init.AsynchPrediv = 127; hrtc.Init.SynchPrediv = 255; hrtc.Init.OutPut = RTC_OUTPUT_DISABLE; hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH; hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN; HAL_RTC_Init(&hrtc);}void HAL_RTC_MspInit(RTC_HandleTypeDef* hrtc){ if(hrtc->Instance==RTC) { /* USER CODE BEGIN RTC_MspInit 0 */ /* USER CODE END RTC_MspInit 0 */ /* Peripheral clock enable */ __HAL_RCC_RTC_ENABLE(); /* Peripheral interrupt init*/ HAL_NVIC_SetPriority(RTC_WKUP_IRQn, 0, 0); HAL_NVIC_EnableIRQ(RTC_WKUP_IRQn); /* USER CODE BEGIN RTC_MspInit 1 */ /* USER CODE END RTC_MspInit 1 */ }} #rtc #wakeup #timer #stm322016-02-24 9:48 AM
Try changing the clock source for the WUT:
HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, ALARM_TIMER,
RTC_WAKEUPCLOCK_RTCCLK_DIV16);
For:HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, ALARM_TIMER,
RTC_WAKEUPCLOCK_CK_SPRE_16BITS);
Let me know!2016-02-29 10:16 AM
Hi eclipsePhage,
The AsynchPrediv and synchPrediv that you are using are dedicated to LSE. In case of LSI, Try to use (AsynchPrediv = 124, synchPrediv = 295). [with STM32F2xx and STM32F4xx] Onother detail, you should clear all the flags just before entering the standby mode. (after HAL_RTCex_SetWakeUpTimer_IT() ) -Hannibal-We’re moving the ST Community to a new platform to give you a better and more reliable community experience.