2013-02-08 10:35 PM
hello every one
i use stm32f107 and i want to use freeRtos and usart1,usart2 interrupts at the same time (only RXNE interrupt) but ofter many usarts interrupt micro controller get fault if i remove usarts interrupts or freertos the program work correctly how can i fix this the priority of usarts tasks is the same ( 1UL | portPRIVILEGE _BIT) and the priority of usart1 interrupt is 44 and the priority of usart2 interrupt is 45 thanks for helping me2013-02-09 6:08 AM
how can i fix this
Use a debugger? You need to better understand the CPU state when it faulted. What instruction, what register settings, what stack state.2013-02-12 5:34 AM
thanks for your replay clive1
i change freertos to rtx and same problem my debugger is keil and the stack size iz 0x2000 and each stack size is 600 and there is three task the program stoped in line 334 of startup_stm32f10x_cl.s //--------------------- DMA2_Channel1_IRQHandler DMA2_Channel2_IRQHandler DMA2_Channel3_IRQHandler DMA2_Channel4_IRQHandler DMA2_Channel5_IRQHandler ETH_IRQHandler ETH_WKUP_IRQHandler CAN2_TX_IRQHandler CAN2_RX0_IRQHandler CAN2_RX1_IRQHandler CAN2_SCE_IRQHandler OTG_FS_IRQHandlerB .
ENDP ALIGN //-------------------------------------------- thansk2013-02-12 7:44 AM
At a guess I'd say you haven't created a USART1_IRQHandler() or USART2_IRQHandler() and it is dumping into the unhandled interrupt routine.
If you changed the names in the vector table, you'd want to confirm the linkage.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.