2015-03-11 12:34 PM
Hi,
I'm new to LwIP and I'm trying to run it on STM32F4 Discovery with FreeRTOS. I'm using STM32CubeMX for generating default code and System Workbench (AC6) as IDE. I use DP83848 PHY in RMII mode. All the software works great (e.g pinging the board, or run the web server demo) if no FreeRTOS is used. But when I add FreeRTOS the board does not acquire a valid IP (either via DHCP or with static IP) so it is not possible to ping the board. This even if I do not add any code to the STM32Cube generated code Thanks in advance if you can help me2015-03-15 11:35 AM
Problem solved.
Simply add this line to lwipopts.h (1000 or whatewer value but > 0): #define TCPIP_THREAD_STACKSIZE 1000If not specified, the default value is 0 (see opt.h) but in that case no lwIp threads is created: this not seems normal for me if I want to use an RTOS.Comments are welcome2015-04-18 7:19 AM
Faced with a similar problem ...
STM32F429 + RTOS + LWIPHelped.My thanks :)Half a day trying to deal with the problem ...Yes, I agree.It would be necessary in the cube to fix something for default settings LWIP + RTOS.2015-04-23 5:42 AM
You are right, in the next STM32CubeMX release, the default value of TCPIP_THREAD_STACKSIZE will be different than zero to avoid the problem you encountered.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.