2023-09-18 9:45 AM - edited 2024-01-20 5:00 AM
Hi
Earlier today I was demonstrating a IAP functionallity with dualbanking on a stm32G474RET. I was saying that it cannot fail as I check the written image with a CRC after it has been written to the new bank.
As I power of the system mid transfer and power it up again, I experience the what we now all expect. It obviously failed.
My system no longer boots normally and as i start to debug it i see that i get a NMI. Now, I unfortunately did not record all the relevant register values, but i am pretty sure that what was set was FLASH_ECCR, bit ECCD. I know this because i see that the NMI trigger as i am doing a boot blank check and CRC on both my banks and the NMI triggers while i am reading from the bank i was writing to.
I have now written a suitable NMI handler to deal with this situation in the future, but how can I intentionally force a double ECC error in a given address in flash?
Best regards
Martin
Solved! Go to Solution.
2023-09-18 9:59 AM
Some discussion and good ideas here:
2023-09-18 9:59 AM
Some discussion and good ideas here:
2023-09-26 12:06 AM
Hi TDK and thanks for the suggestion.
I ended up doing the same thing as that thread suggested. After around 60 attempts cut power while programming the flash, the error triggered.
I got "lucky" after that and the next time i needed to trigger it it took only 27 attempts.
// Martin
2023-09-26 7:25 AM
Haha, well thanks for reporting back. Good to know it works even if it's a bit time consuming to test. Wonder if it's a timing thing, where if you cut power at the exact same time relative to programming, it would happen every time. Just guessing.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.