2012-09-01 5:33 AM
Hello, i want to boost DFT speed so i need to calculate lot of sinf cosf and store in external SRAM. internal is capable only for few dft points in spectrum, so i have to store them into SRAM, but don't know how to do that.
it work fine for 16b integers (i have 8Mb organized as 16b blocks) i have this functions to read/write: void SRAM_Write(uint16_t data, uint32_t WriteAddr); int SRAM_Read(uint32_t ReadAddr);2012-09-01 7:12 AM
The floats would be 32-bit IEEE 754 format.
float convert_u32_to_float(uint32_t x) { return(*((float *)&x)); } The bigger question is why you don't access the external memory directly, as it's presumably parked in the middle of the ARM's address space and directly accessible. float *array_of_floats = (float *)0x60000000;We’re moving the ST Community to a new platform to give you a better and more reliable community experience.