2013-05-16 9:53 AM
I have a project where I will need to flash a few hundred chips that are already on boards. I have set up a chain programmer which is controlled by an MCU. basically it is just a chain of sockets for the boards that all get connected to an st-link v2, and it sequentially powers up the boards and runs a bat file to flash them. But I cant seem to find any information on using the st-link utility in windows command line. I use it linux, but this project will be used by our assembly department and they all run windows 7.
Does anyone have any information on using the st-flash in command line on windows?2013-06-05 2:41 AM
http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/CD00262073.pdf
for more details on how to do it. Regards, ST.MCUTo give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.