2019-01-10 11:31 PM
Hello,
In stm32h7 I find examples/FLASH/WriteProtection example in EVAL folder, but the same example is missing from Nucleo folder.
The protection is for the user flash (internal flash), so why is it missing from Nucleo ?
(I rather do it in NUCLEO, so that if I get into unrecoverable flash, I will still have the more expensive EVAL board with me...)
Thanks,
Ran
Solved! Go to Solution.
2019-01-10 11:48 PM
The examples are not exactly extensive, the expectation is that you'll port or create what you actually need.
2019-01-10 11:48 PM
The examples are not exactly extensive, the expectation is that you'll port or create what you actually need.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.