2009-08-12 12:28 AM
Flash update using CAN on STM32F103
2011-05-17 4:20 AM
Hi
I am currently looking at reducing the component count on a PCB which use a STM32F103 micro, am considering remove the USART as its only function is to provide a method to update the flash. I see that the CAN port can be used to perform this operation on the STM32F105 and 7 micros (AN2662), is this also possible of the STM32F103 micro? If so how can this be achieved? Thanks IanWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.