2024-03-28 7:15 PM
Hi there,
I am working on a project using the STM32H755 zi that has 1 USBC port, can we use the same port for uploading the code, UART Communication and powering the device instead of using ST-LINK? Or is there any way to use ST-LINK for communication?
Thanks for any help.
Solved! Go to Solution.
2024-03-28 7:25 PM
You could use the ST-LINK VCP to communicate with loader code on the H755, and upload firmware via a terminal supporting X/Y-MODEM. Perhaps look for some of the STM32 IAP examples.
Not sure it's connected to the UART supported by the System Loader, see AN2606 / AN3155
Otherwise you might try the other USB connection
2024-03-28 7:25 PM
You could use the ST-LINK VCP to communicate with loader code on the H755, and upload firmware via a terminal supporting X/Y-MODEM. Perhaps look for some of the STM32 IAP examples.
Not sure it's connected to the UART supported by the System Loader, see AN2606 / AN3155
Otherwise you might try the other USB connection
2024-03-29 3:52 AM
Hello @isaacjack
If you need a Flash disk to upgrade your device, you can refer to AN3354 as an example.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.