cancel
Showing results for 
Search instead for 
Did you mean: 

FLASH_pageErase on stm32F030X8

v2399
Associate
Posted on November 17, 2016 at 10:35

Hello everybody,

I'm actually working on a bootloader on an STM32F030X8 board. The programme already work's on a L100RC and an F303RE.

My bootloader starts at 0X08000000 ans my user app starts at 0X0800FA00.

I need to eraser before writing so here is what i do :

for(i=pStartAdress_u32;i<pEndAdress_u32;i+=1000)

    {

        halFlashPageErase_v((u8 *)i);

    }

with start = 0x0800FA00 and end = 0x0803E800

the + 1000 is because page size is 1KB

then hal calls drivers with this function :

void drvFlashPageErase_v(u8 * pAddress_u8)

{

    HAL_FLASH_Unlock();

    FLASH_PageErase((u32)pAddress_u8);

    HAL_FLASH_Lock();

}

My probleme is when i call this my programme blocks and my stack shows this :

Thread #1 (Suspended : Signal : SIGINT:Interrupt)

0xfffffffe

<signal handler called>() at 0xfffffff1

0xfffffffe

<signal handler called>() at 0xfffffff9

drvFlashPageErase_v() at drvFlash.c:80 0x8003780

halFlashPageErase_v() at halFlash.c:70 0x80047fc

sSvcComProtFlashErase_b() at svcComProt.c:723 0x8006490

sCmdErase_v() at svcComProt.c:395 0x8005e60

sSvcComProtHandleCommand_u8() at svcComProt.c:972 0x800698a

svcComProtBootProcess_v() at svcComProt.c:1 092 0x8006b4a

<...more frames...>
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
slimen
Senior
Posted on December 01, 2016 at 12:00

Hello,

May be this example can help you, it describes how to configure and use the

 FLASH HAL API to erase and program the FLASH memory:

STM32Cube_FW_F0_V1.6.0\Projects\STM32F072B-Discovery\Examples\FLASH\FLASH_EraseProgram

Regards

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.