2007-11-07 7:19 PM
Flash and Ram size
2011-05-17 3:17 AM
Is there a method to know the Flash size and/or the Ram size for the device which execute a code ? Perhaps with register MMFRx in Cortex-M3 system ? But these registers are not documented.
alternately, is there a register with an unique ID for a STM32 device reference ? I want to develop an universal Boot Loader for all the STM32 and I want this Boot Loader can send an error code if adress to program is too large for a particular device. Thank you EricWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.